Interpolation time period (interpolation time units)
| Index.Sub | 60C2.1H |
| Data Type | Unsigned8 |
| Access | Read/Write |
| PDO Mappable | RX_PDO (1) |
| Unit | -- |
|
Range |
-- |
| Default Value | 1 |
| Store Supported | Yes (2) |
| Description |
This object is used to define for interpolation period computation : Interpolation time period = Interpolation_time_units * 10 Interpolation_time_index seconds |
|
Notes |
(1) available with firmware V03r03 or superior. (2) ‘Store supported’ is available with firmware V01r36 or superior. See Interpolation time period (interpolation time index) (60C2.2H) object. |